NX Feature List of Renew Feature is empty or not showing expected feature

2021-10-06T23:26:56Z
NX for Design

Summary


Details

Renew Feature is not showing feature to be upgraded. Why is the Feature List is empty? Why is a certain feature not showing up in the Feature List?



Solution

In NX11.0, the following features from previous NX release are supported by Renew Feature:


Edge Blend 
Offset Curve in Face 
Trim Body 
Face Blend 
Offset Surface 
Blend Corner 
Intersection Curve 
Thicken 
Draft Body 
Law Extension 
Trim and Extend 
Fill Surface 
Split Body 
Variational Sweep 
Trim Sheet 
Combined Curve Projection


Additional features will be made available in future NX releases.


Also note that features created earlier than NX8 are not supported by Renew Feature.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V11.0
Function: ARCHITECTURE

Ref: 002-7008141

KB Article ID# PL7008141

Contents

SummaryDetails

Associated Components

Modeling