How to change the preselection and selection colors in NX?

2021-10-06T23:27:07Z

Summary


Details

Some users may be color blind and cannot notice the difference between the default red (preselection) and orange (selection).

Solution

The following steps can be used to change the colors manually:


  1. Go to File --> Preferences --> Visualization. 
  2. Select [+] Color from the menu on the left of the Visualization Preferences dialog box.  The General sub category is selected where one can choose Geometry Colors for Preselection and Selection, amongst others.  Note also the Drawing Layouts sub category which also has Preselection and Selection color choices.


Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: SYSENG
Version: V1847
Function: VISUALIZATION

Ref: 002-7008069

KB Article ID# PL7008069

Contents

SummaryDetails

Associated Components