NX If I run NX 1847 and NX 1859 at the same time, are 2 gateways consumed?

2021-10-06T23:27:17Z
NX System Administration

Summary


Details

--------------- 
If I run 2 NX sessions from the same "computer + display + user account", it 
will only consume one "gateway" license.


But if I do that, and look at the license server log file, I see 2 lines, so 
it is hard to know what is really going on.


15:35:28 (ugslmd) OUT: "gateway" boo@<serverhostname> ! NX 1847 session
15:35:51 (ugslmd) OUT: "gateway" boo@<serverhostname> ! NX 1859 session




Solution

 Flexlm server log file, splm_ugslmd.log logs all transactions.


A transaction indicates that a request (from client) was either satisfied or 
denied.


A license request from client can be classified as either "hard" or "soft".


Rules encoded inside the ugslmd deamon determine classifications.


In the case of NX, ugslmd will only consider the 1st request from a particular 
"computer + display + user account" to be a hard request.


Also subsequent requests from identical computer + display + user account to 
be classified as soft requests and thus not tallied against outstanding 
license feature count.


To verify:


lmutil lmstat -f gateway -c 28000@<server hostname> | more


Will produce a listing similar to: (NOTE: edited for clarity)


Users of gateway: (Total of 10000 licenses issued; Total of 82 licenses in 
use


Starting of additional sessions of NX of any version in identical computer + 
display + user account will *not* change license usage.



Notes and References

IR7518685



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 1064
Product: NX
Application: SYSENG
Version: V1847
Function: SYSTEM_TOOLS

Ref: 002-7007994

KB Article ID# PL7007994

Contents

SummaryDetails

Associated Components

Installation