Export PDF in Modeling Does Not Capture Shaded Image

2021-10-06T23:27:06Z

Summary


Details

Export PDF in Modeling Does Not Capture Shaded Image.



Solution

 Using 'File -> Export -> PDF' command creates a CGM (Computer Graphics Metafile) file before passing it into a converter to generate the PDF. CGM's are wireframe only data (except if it is a Drafting member view with shaded image in a Drawing Sheet).


But, if you need a shaded image capturing a Modeling view, use 'File -> Print' and set the 'Output' option to shaded, and send it to a PDF file. This requires a user to have the Adobe PDF printer installed on your operating system.


Capturing the shaded model image is this manner will also capture displayed object attributes, temporary markers, etc. along with all objects displayed on screen while in Modeling.

Notes and References

This applies to all NX releases.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: GATEWAY
Version: V11.0
Function: PDF

Ref: 002-7007957

KB Article ID# PL7007957

Contents

SummaryDetails

Associated Components