During upload of robot program, dialog box "Mfg container" appears even if Tecnomatix doctor GUI is set as "Create as Private".
Solution
The Tecnomatix doctor GUI (Located under Tools --> Teamcenter Mapping Configuration in the Tecnomatix Doctor) is used to modify the TcPsMappingConfiguration.xml file. When the file has been manually modified and illegal "Type" syntax has been added and not recognized, the result is a dialog box that says "Mfg container".
The fix to this is use legal "Type" syntax.
Here is the legal recognized list of "Types":
<Type>ArcWeld</Type>
<Type>Seal</Type>
<Type>LaserWeld</Type>
<Type>LaserCut</Type>
<Type>WaterJetCut</Type>
<Type>RollerHemming</Type>
<Type>Paint</Type>
<Type>LaserBraze</Type>
<Type>Machining</Type>
<Type>Coating</Type>
<Type>PlyLayup</Type>
<Type>Glue</Type>
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V14.1.1
Function: BACKBONE_INTEG
Ref: 002-7007908