---------------
You may have the use case where you need to drive the value of an NX string expression from a cell in the NX spreadsheet. You have created the string expression in NX and then used the NX spreadsheet --> Add-Ins --> Extract Expr tool to bring the expression into the spreadsheet.

Solution
In the cell (B4 here) that will be driving NX use the following string:
CONCATENATE("""",C4,"""")
where cell C4 is the cell with the string value you want to send back to NX

Cell B4 will show the contents in quotes but it will correctly update the NX
part when "Update NX Part" is performed after selecting your choice in the
drop down menu.
The value in the Expression dialog will now be updated to the string value specified in the spreadsheet

Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1847
Function: EXPRESSION
Ref: 002-7007885