NX XLS file and KRK are not copied during clone operation using Add Reuse Dialog.

2021-10-06T23:27:10Z
NX for Design

Summary


Details

--------------- 
The problem is XLS file and KRK are not copied when we perform clone 
operation in Add Reuse component dialog which contains only UGMaster dataset.



Solution

 The problem where XLS file and KRK are not copied when we perform clone 
operation in Add Reuse dialog can be addressed as shown below.


Before NX10, when perform clone operation in Add Reuse component dialog 
which contains only UGMaster dataset, set the environment variable 
UGII_REUSE_LIBRARY_CLONE=YES the XLS file will copy to new dataset.


From NX10 and later version, the clone option method can be set "Use Clone 
Assembly" or "Use File Save As" in customer defaults(Gateway->Reuse 
Library->Reusable Component->Part Copy Method), the xls file can be copied to 
new dataset.



Notes and References

IR 7574144



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: KDA
Version: V7.5.5
Function: REUSE_LIBRARY

Ref: 002-7007879

KB Article ID# PL7007879

Contents

SummaryDetails

Associated Components

Drafting Modeling