NX Prevent MVStyle in JT Files Created From NX10 and Later Versus Earlier NX Releases.

2021-10-06T23:26:58Z
NX for Design

Summary


Details

Prevent MVStyle Found in JT Files Created in NX10 and Later Versus Earlier NX Releases.



Solution

The JT Files MVStyle PMI in model view was introduced in NX10.0.3.


The JT translator started to support all types of NX model view rendering styles (such as Shaded, Shaded with edges, etc.) in JT and the MVStyle PMI stores these rendering styles within the JT file.


There is no way to prevent the NX views and the MVStyle PMI data from being translated into a JT file, because the new capability works by default without any configuration control.

In Teamcenter Visualization V11.3 and earlier releases initially reported the MVStyle PMI which was displayed in the PMI tree as well in each Model View which can confuse users because it is not reported within NX. Teamcenter Visualization V11.4 and V12 was changed and now even if MVStyle PMI is present in a JT, it is no longer shown in the PMI navigator.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: PMI
Version: V10.0
Function: JT_OUTPUT

Ref: 002-7007877

KB Article ID# PL7007877

Contents

SummaryDetails

Associated Components

PMI