Details
---------------
How to convert "blank space" to "_" during export.
Solution
Set the following variable.
As the variable name suggests it helps in converting SPACE -> UNDERSCORE.
The variable can be set at user or system level in the Windows Environment
Variables dialog, or it can be added to the ugii_env.dat file:
UGII_CLONE_SPACE_UNDERSCORE_CONVERSION=true
Note: All the parts with "/" character will be automatically exported with "_"
conversion as parts with "/" are not supported on Windows.
Notes and References
IR/PR 7668775
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V7.5.5
Function: CLONE_EXPORT
Ref: 002-7007859