How to change line thickness of one segment in a drafting view/drawing

2021-10-06T23:26:52Z

Summary


Details

To edit the Width or Style of all lines in a drawing, the drafting preferences can be modified to make the desired changes. However, it is sometimes necessary to change the Width or Style of only certain lines in a view.



Solution

In order to change the Line Width or Style, the following steps can be followed:


  1. Right click the view containing the desired line for editing and click View Dependent Edit. 
  2. Under the Add Edits options click Edit Entire Objects. 
  3. Under Wireframe Edits, choose desired Line Width and/or Style. 
  4. Click Apply. 
  5. Click the objects desired. 
  6. Click OK in the Class Selection window. 
  7. Click OK again in the View Dependent Edit window.


Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V1847
Function: DRAWING/VIEW

Ref: 002-7007723

KB Article ID# PL7007723

Contents

SummaryDetails

Associated Components