---------------
When we trying to Publish created 2D Components in "Local 2D Components" folder
then "No Published 2D Component Libraries exist" warning message displayed.
Solution
When we not define link of 2D Component Libraries in Customer Defaults this
warning message is displayed.
To avoid this warning message we need to define 2D Component Libraries path as
shown in below Customer Defaults.
Example:-
1. Create one 2D Component Libraries folder.
[Example: In "D" drive created one folder as "2D_Component”].
2. Goto, File -> Utilities -> Customer Defaults ->Gateway -> Reuse Library: 2D
Component Library.
In Native NX:
We need to set the path of the folder as shown below.
2D_Component|D:\2D_Component.
Note: This Field specifies the 2D Component libraries in native NX. Each Line
defines a 2D Component library; the string before "|" is the library name, the
string after is the path.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 764
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: 2D_LAYOUT
Ref: 002-7007564