The behavior of the section/projected view has changed from NX 10.0.2.

2021-10-06T23:27:15Z

Summary


Details

--------------- 
The behavior of the section/projected view has changed from NX 10.0.2.



Solution

 The behavior of the section/projected view has changed from NX 10.0.2. 
 [Insert] -> [View] -> [Section]/[Projected].


 <Placement: Method> is set to the "hinge" by default.


Added New “Hinge” option to Placement method in View Origin group similar to 
projected view dialog. Make “Hinge” default placement method i.e., 
• Honor the Associative Alignment preference when it is on and make the 
Hinge Method the initial value for section views. 
• If Associative Alignment preference is off, follow dialog memory, but 
hinge can be the initial value rather than inferred.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764
Product: NX
Application: DRAFTING
Version: V11.0.1
Function: DRAWING/VIEW

Ref: 002-7007464

KB Article ID# PL7007464

Contents

SummaryDetails

Associated Components