NX How does "Align to hinge" works with "Hinge" option in Drafting in NX10.0.2.

2021-10-06T23:26:42Z
NX for Design

Summary


Details

--------------- 
The behavior of the section and projected view has changed from NX 10.0.2. 
 [Insert] -> [View] -> [Section]/[Projected].


 <Placement: Method> is set to the hinge by default.


 The problem, if we have selected the "Hinge" as the selected method, we can 
not use the "Align to hinge" option, change the same to Infered to get the 
Align to Hinge option with MB3 selection.



Solution

 When We launch section/ projected view dialog, change hinge placement method 
to Infered and now use MB3 to select "Align to Hinge” to place the view with 
the freezed current location.



Notes and References

IR7522815



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764
Product: NX
Application: DRAFTING
Version: V10.0.2
Function: DRAWING/VIEW

Ref: 002-7007463

KB Article ID# PL7007463

Contents

SummaryDetails

Associated Components

Drafting