About the character limitation of ugmanager clone

2021-10-06T23:26:45Z

Summary


Details

--------------- 
About the character limitation of ugmanager clone


Steps to reproduce the problem 
 1) Please create an Item with following ID.


MAXIDTEST_1238456789_123456789_123456789_123456789_123456789_123456789_12345678 
9_123456789_123456789_1234567


 2) Please create the dataset of Non-master drawing part with same ID. 
 3) Try to export it with ugmanager clone as following.


 D:\App\NX\NX10014\UGMANAGER>ugmanager_clone -pim=yes -u=infodba -p=infodba 
-o=export -default_n=autotranslate -copy_n=specification:yes 


-asse="@DB/MAXIDTEST_1238456789_123456789_123456789_123456789_123456789_1234567 
89_123456789_123456789_123456789_1234567/A"


 -> following error occurs.


ERROR: (640162) - Filename is too long 
 While performing export 
 This error occurred while operating on the part 
@DB/MAXIDTEST_1238456789 
_123456789_123456789_123456789_123456789_123456789_123456789_123456789_12345678 

_1234567/A/specification/MAXIDTEST_1238456789_123456789_123456789_123456789_123 

56789_123456789_123456789_123456789_123456789_1234567-A-dwg1



Solution

 There is a character limitation of the file name of NX part file on the Native 
Disk. 
The limit is around 256 characters including the full path of the part stored 
location. 
The moment the UGPart file is added in the Item and tried to export it it 
reaches the limit of the characters and gives an error message. 
This is a Microsoft Windows limitation for any part file name.



Notes and References

IR 7461815



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V10.0.1
Function: CLONE_EXPORT

Ref: 002-7007414

KB Article ID# PL7007414

Contents

SummaryDetails

Associated Components