Move The Position Of A Dimension's Value Between Its Extension Lines

2021-10-06T23:27:15Z

Summary


Details

Having inserted a dimension on a drawing how do you move the dimensions value so that it appears between the arrows.  This used to be called Manual Placement - Arrows Out/In.



Solution

  1. Right click the dimension and select Settings. 
  2. Expand [+] Line/Arrow from the list on the left. 
  3. Select Arrowhead. 
  4. In the section on the right titled Workflow uncheck Automatic Orientation. 
    Once unchecked you can manually place the dimension as desired.


Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V1847
Function: DIMENSION

Ref: 002-7007397

KB Article ID# PL7007397

Contents

SummaryDetails

Associated Components