A Radial Bend Shape Segment has been applied to a branch on a Formboard. However, having reviewed the Formboard in drafting it was decided that the Shape Segment needsto be removed but there is no option to delete it.
Solution
Open the Shape Segment command and pick the branch where the Shape Segment has been applied. The command will recognize that the Radial Bend Type has been used on that branch. The user can then change the Type from Radial Bend to Line and apply the change, which removes the pivot points from the previous type.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: ROUTING_ELEC
Version: V1847
Function: FORMBOARD_V2
Ref: 002-7007390