Newly Added Curve Text Does Not Display At Higher Level Assembly

2021-10-06T23:26:39Z

Summary


Details

Having made a component the work part and added Curve Text to the component, the text disappears when making the parent assembly the work part.



Solution

Geometry displayed at the Assembly level is controlled by several display parameters, such as Layers, Reference Sets and View Dependency.


The most likely reason for the Curve Text not displaying is that the component has been set to the MODEL reference set at the assembly level.


Curve geometry, unlike Solid geometry, is not automatically added to the MODEL Reference Set.  Make the component the work part and select Menu --> Format --> Reference Sets.  Highlight the MODEL Reference Set and select the text to add it to the Reference Set.  Make the assembly the work part and the text 
should now display.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: ASSEMBLIES
Version: V1847
Function: ASSEMBLY_MODEL

Ref: 002-7007389

KB Article ID# PL7007389

Contents

SummaryDetails

Associated Components