Removing An Assigned Material From A Body

2021-10-06T23:27:03Z

Summary


Details

Having assigned a material to a body, how do you remove it?



Solution

 Select Tools --> Materials --> Manage Materials.


The dialog defaults to Library Materials. The currently assigned material is identified by the green check in the Used column.


Change the pull down at the top of the dialog to Local Materials to see a list of materials used in the part.


Right click the material to be removed and choose either Remove Usages, which removes the material from the assigned bodies, or Delete, which removes the material from the Local Materials.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: ASSEMBLIES
Version: V1847
Function: ASSEMBLY_MODEL

Ref: 002-7007387

KB Article ID# PL7007387

Contents

SummaryDetails

Associated Components