Simcenter 3D Solutions Why can't I create plane strain elements in a fem?

2021-10-06T23:27:18Z
Simcenter 3D

Summary


Details

--------------- 

When using 2d mesh in an NX Nastran fem, I do not see plane strain (cplstn) or 

plane stress (cplsts) elements as an option for element type.

Solution

 In order to mesh these types of elements, the fem 2d solid option must be 

defined. Use right mouse button, edit, on the name of the fem at the top of the 

simulation navigator and set the 2d solid option to zx plane or xy plane.

Notes

KB Article ID# PL7007221

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow