Simcenter 3D Solutions Stress Wizard doesn't show any bodies when starting a new simulation.

2021-10-06T23:26:45Z
Simcenter 3D

Summary


Details

--------------- 

After I start Stress Wizard and open a .sim file, the graphics area is blank 

and I can't select a body to analyze.

Solution

 Stress wizard can only analyze solid bodies, not sheet bodies. Make sure there 

is a least one solid body in the active part file.

Notes

KB Article ID# PL7007220

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow