Plant Simulation Nothing flows in simple PlantSimulation Fluid model

2021-10-07T00:01:46Z
Plant Simulation

Summary


Details

A simple model consisting af a FluidSource, Pipe, and FluidDrain does not simulate fluids flowing when the simulation is started. The clock never advances past 0.

Solution

If one creates simple models consisting of:


Source, Pipe, Sink 
Source, Pipe, Tank, Pipe, Sink


The simple fluid simulations do nothing unless an object that consumes time is inserted. 


Without this object, the time never advances past 0:00:00 and a trace shows:


 Init 0.0000 .Models.Frame.EventController 
 StartActions 0.0000 .Models.Frame.FluidSource


The Source, Pipe, Tank, and Sink do not consume time for fluids.


A Source normally produces a widget every X amount of time. The Source in this case consumes time when it creates a widget and logs an event to get rid of its production. Advance the clock to process the event and away the simulation goes.


When simulating liquids, a Source (pump) produces continuously. The choice being an infinite number of events or no events. Infinity is difficult to simulate, so the choice is no events. The same is true for a tank or a pipe.


Adding a Mixer or any other Object that has a processing time will consume time and cause the clock to advance. The fluid simple simulation will run.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: TECNOMATIX
Application: PLANTSIMULATION
Version: V13.1.X
Function: ALL

Ref: 002-7007213

KB Article ID# PL7007213

Contents

SummaryDetails

Associated Components

Application Education Gantt Chart General Interface Package Professional Runtime Standard VSM Library