Is it possible to automatically create the
IPW in a background process immediately after an operation is generated?

Solution
A
Customer Default was added that will cause
NX to transparently create the
IPW as a background process after the tool path is generated. This variable can be enabled by going to
File -> Utilities -> Customer Defaults -> Manufacturing -> Operation -> Automatically Generate IPW in Background.

Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1859
Function: BASIC_FUNCTIONS
Ref: 002-7007168