Customer upgraded multiple hosts to NX/1847 Series.
Customer hosts could all plot without issues until single user on single host
plot operations failed without warning.
When single user on single host attempts to plot the following error is
raised:
Printer Groups Error
Directory is not accessible because of the following error:
Plotting directory is not writable.

Solution
ANALYSIS:Inspection of users .syslog indicates the following:
UGII_SDI_OUTPUT_DIR = C:\Users\<username>\AppData\Local\Temp
Users ...\Temp directory was permanently locked by external mechanism,
(probably by 3rd party product which shares directory structure) and therefore
was rendered not writable by SDI plot subsystem during attempted creation of
intermediate plot files.
SOLUTION:
Need to delete C:\Users\<username>\AppData\Local\Temp and all contents.
(C:\Users\<username>\AppData\Local\Temp will automatically be recreated by
Windows).
Additional Suggestions:
Run Windows File system cleanup utility after directory deletion.
Reboot host.
Notes and References
IR7432339
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 1064
Product: NX
Application: SYSENG
Version: V1847
Function: INSTALL_ISSUES
Ref: 002-7007042