NX What are the Motion Envelope Quality tolerance settings?

2021-10-06T23:27:16Z
NX for Design

Summary


Details

--------------- 
The Motion Envelopment Quality setting for "Envelope Accuracy" has 4 options


 Low 
 Medium 
 High 
 Custom = .005 (default envelope tolerance)


If the User wants to use the "Custom" option and enters a value, they're 
not sure if the value is close to, Medium, Low or the High setting. What are 
the Envelope tolerances values for Low, Medium, & High?



Solution

 The Tolerance values for the Low, Medium and High Envelope Accuracy are;


 Low = 0.005 
 Medium = 0.003 
 High = 0.001



Notes and References

IR7348427



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V9.0
Function: SEQUENCING

Ref: 002-7006850

KB Article ID# PL7006850

Contents

SummaryDetails

Associated Components

Assemblies