NX Balloon does not update with the Parts List Callout number.

2021-10-06T23:26:48Z
NX for Design

Summary


Details

--------------- 
After adding a Balloon to an edge of a component, updating the parts list does 
not update the balloon with the callout number in the Parts List.



Solution

 One of the reason could be the Environment Variable is set for 
"UGII_UPDATE_ALL_ID_SYMBOLS_WITH_PLIST=0". To verify if the variable is set. go to File --> Help --> 
Log File and search for the Environment Variable. If it is set, have your 
system administrator either delete that variable or change the value to 1.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V9.0
Function: TABLES

Ref: 002-7006849

KB Article ID# PL7006849

Contents

SummaryDetails

Associated Components

Drafting