How to break curve of the view, if curve and Note is overlap.

2021-10-06T23:27:08Z

Summary


Details

--------------- 
User wants to break curves if curve and Notes are overlapped in View.



Solution

 Use "View Dependent Edit command Edit Object Segment" option to break solid 
line.


Refer below Steps to break view curves. 
-------- 
1. Select View -> MB3 -> Active Sketch. 
2. Create two lines to define cut portion on curve to break View -> Finish 
Sketch. 
3. Select View -> MB3 -> View Dependent Edit. 
4. Select option "Edit Object Segment: Line Font set as Invisible" -> 
Apply. 
5. Select line to edit [Which you want to break]. 
6. Select bounding objects1 and 2 -> OK. 
7. Close Edit object segments dialog Box and View Dependent Edit dialog 
Box. 
8. Select Sketch and Delete.


You will get Break potion of the curve.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764
Product: NX
Application: DRAFTING
Version: V9.0.3
Function: DRAWING/VIEW

Ref: 002-7006790

KB Article ID# PL7006790

Contents

SummaryDetails

Associated Components