How to use DXF file for 2D Layout

2021-10-06T23:26:53Z

Summary


Details

--------------- 
When we try to add Existing Curves of the DXF geometry for 2D layout we cannot 
select them. we need to make the sketch as an active to add curves.



Solution

 Workaround: 


i). Import the DXF file to Drafting as sketch curves (setting the appropriate 
Import options). 
Steps to Import DXF File. 
1. File -> Import ->AutoCAD DXF/DWG. 
2. Select DXF file to import as a New part. 
3. Options: Drawing View -> Finish. 
Drawing Views are imported as a Sketch.


ii). Using 'Define' command to create the 2D components instead of using 'New' 
command to add existing curves from the active sketch.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764
Product: NX
Application: DRAFTING
Version: V9.0.3
Function: TRANSLATOR

Ref: 002-7006753

KB Article ID# PL7006753

Contents

SummaryDetails

Associated Components