---------------
Open
NX11 and run
Convert Tool Library by selecting the
tool_database.dat from an
NX10 english or metric library. The error message seen below is reported. What can be done to work-around this issue?

Solution
This issue is caused by tab characters in a few
#CLASS records in the
NX10 english and
metric versions of
tool_database.dat. These characters can be manually deleted out of the two files allowing the upgrade to succeed. The records to modify are the
#CLASS STD_LASER and
#CLASS DEPOSITION_LASER records in the english version and
#CLASS DEPOSITION_LASER in the metric version.

Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V11.0.2
Function: LIBRARIES
Ref: 002-7006698