NX Assembly components are invisible

2021-10-06T23:26:44Z
NX for Design

Summary


Details

--------------- 
An assembly component cannot be made visible by toggling on in the assembly navigator.



Solution

In this case, the user had hidden the solid bodies rather than the component part. Normally, without a filter selected, just picking 'Hide' and picking the geometry on the screen should hide the component part. For some reason, the user had hidden the solid body within the component part


'menu - edit - show & hide - Invert shown & hidden' (or Ctrl+Shift+B) 
This displays the hidden solid bodies - which can then be made visible.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V10.0
Function: ASSEMBLY_MODEL

Ref: 002-7006551

KB Article ID# PL7006551

Contents

SummaryDetails

Associated Components

Assemblies