NXCAM postprocessing - Tap output is always MMPM

2021-10-06T23:26:55Z

Summary


Details

--------------- 
When postprocessing, Tap output is always MMPM. It should be MMPR.



Solution

Postbuilder: Program & Tool Path --> Program --> Tool Path --> Machine Control. Click on Feedrates and set the Cycle Feed Rate Mode to "Auto". This will make the post output the setting that was made in the operation.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0
Function: POSTBUILDER

Ref: 002-7006549

KB Article ID# PL7006549

Contents

SummaryDetails

Associated Components