NX "Delete Unused Expressions" deletes expressions used in PTS template

2021-10-06T23:27:15Z
NX for Design

Summary


Details

--------------- 
Using File --> Utilites --> Part Cleanup --> Delete unused expressions, will 
delete expressions that are used in the PTS template



Solution

 For this type of expressions the PTS dialog only has code to read the value of 
the expression and display it in the dialog. From the NX point of view this 
expression is unused - and therefore it will be removed with the cleanup 
function.


The only workaround would be to use some clever method in part preparation for 
PTS where the expression could be referenced in some way so that the part would 
be "safe" for cleanup of unused expressions.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V8.5
Function: PART_FILE_OPS

Ref: 002-7006297

KB Article ID# PL7006297

Contents

SummaryDetails

Associated Components

Assemblies