How do you edit sketch dimensions using the slider bar in NX12?

2021-10-06T23:27:04Z

Summary


Details

--------------- 
Prior to NX9, you can access the sketch dimension dialog which shows you a list 
of all dimensions and you can edit the dimensions using the slider bar. 
How do you get this dialog in NX12 Task Environment sketcher?



Solution

 In NX12, to access the sketcher dimension dialog for the slider bar and the list 
of dimensions the user has to do the following:


1) Double click on the sketch in the work area or the sketch feature in the 
Part Navigator to make the sketch active.


2) Use Mouse Button Three on the highlighted sketch in Part Navigator to access Edit Parameters.

Or Select any sketch dimension on the screen -> RM -> Edit Parameters 
Once Edit Parameters has been selected the Sketch Parameters dialog will 
display and any of the sketch dimensions can be modified with the slider bar.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0.2
Function: SKETCHER

Ref: 002-7006296

KB Article ID# PL7006296

Contents

SummaryDetails

Associated Components