Need to combine faces after importing Step file.

2021-10-06T23:27:01Z

Summary


Details

--------------- 
After a user imported a Step file and sewn into a solid body, all of the 
cylindrical and conical faces were split into separate faces. The faces needed 
to be joined together but the option Join Faces raised an error that there were 
no mergable faces, what other options are there to join those faces.



Solution

 One option would be to use the Synchronouse Modeling option "Optimize face" 
to fix those split faces.


Insert --> Synchronous Modeling --> Optimize --> Optimize face



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V7.5
Function: SYNC_MODEL

Ref: 002-7006292

KB Article ID# PL7006292

Contents

SummaryDetails

Associated Components