Meaning of options from RMB over the field for Prefix in view label?

2021-10-06T23:27:13Z

Summary


Details

While in the Customize Drafting Standard dialog (from File > Utilities > Customer Defaults > Drafting > General, and under the Standard tab, click on Customize Standard), expand "View" and for Base/Drawing, Projected, Section, and Detail, under the Label tab when Right Mouse Button over the field for Prefix, the following three options appears in the popup menu:


 Right to Left Reading order 
 Show Unicode Control Characters 
 Insert Unicode Control Characters


What do these options mean?



Solution

Right to Left Reading order - this can be used for language characters that writes from right to left (Hebrew as an example, opposed to English).


Insert Unicode Control Characters - allows selection of unicode control characters from the listing to be used with the view name; Unicode control characters are tags that help with text flow and direction for languages such as Arabic or Hebrew. If you have multiple languages installed on your computer, you can show Unicode control characters when you right-click any edit control in Windows, such as a text box, or when you use Notepad.


Show Unicode Control Characters - this will display any unicode control characters created with option "Insert Unicode Control Characters".



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: DRAWING/VIEW

Ref: 002-7005925

KB Article ID# PL7005925

Contents

SummaryDetails

Associated Components