Assembly Constraint Are Not Being Saved After Creation

2021-10-06T23:26:49Z

Summary


Details

Having clicked OK or Apply to constrain two components together the newly created positioning constraints are not saved and they are not displayed within the Constraints node of the Assembly Navigator.



Solution

Reopen the Assembly Constraints dialog and expand the Settings block (located at the bottom of the dialog).  Check the status of the Associative option.  If it is unchecked, positioning constraints will not be saved. When Associative is checked, Positioning Constraints will be immediately listed within the 
Constraints node of the Assembly Navigator once Apply or OK has been selected.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: ASSEMBLIES
Version: V1859
Function: POSITIONING

Ref: 002-7005715

KB Article ID# PL7005715

Contents

SummaryDetails

Associated Components