---------------
The menu of the 3D Input device shows menu entries in NX, but they do not show
icons.
Solution
This can be caused by missing bmp files.
Verify if the following icons:
3dxbuttonmapping.bmp
3dxcube_24x24.bmp
3dxhelp.bmp
clear_rotate_point.bmp
are available inside .../ugii/Bitmaps folder.
You also can set the enivronment variable UGII_BITMAP_PATH to the folder where
the bmp files are existing in.
Notes and References
Hardware/Software Configuration
Platform: AMD64
OS: window
OS Version: 764
Product: NX
Application: SYSENG
Function: DEVICES
Ref: 002-7005700