NX starting Relations Browser with NX Teamcenter Integration

2024-04-30T08:55:32Z
NX for Design

Summary


Details

---------------

Relations Browser does not start with NX Teamcenter Integration (NX native

starts)

Solution

1. Install Java7 64bit

2. UGII_JAVA_HOME and UGII_JVM_LIBRARY_DIR must be set, that the relation

browser works.

set

UGII_JAVA_HOME is C:\Program Files\Java\jre7

UGII_JVM_LIBRARY_DIR is C:\Program Files\Java\jre7\bin\server

Important is that this both variables are not overwritten from the TC start

batch files. To prevent it set both variables in start_nxmanager.bat

Additional be sure that there is no space at the end of the value from

UGII_JAVA_HOME

This leads to a path variable problem that prevents the Relations Browser to

start only from NX Manager.

Notes

IR1971636

Notes

KB Article ID# PL7005697

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX