How to configure NX Validation in 4tier mode

2024-04-30T08:41:05Z

Summary


Details

---------------

This article describes how to configure NX Validation in 4tier mode to run

validations from Teamcenter about Tools - Validation - Run Validations...

Solution

1. set "Is Client Utility" to True:

In TC open Validation Manager, select NX Check-Mate Item under Validation Home,

right mouse button Edit properties If the Is Client Utility property is set to True, the tool defines the

application/ugcheckpart MIME type. You must perform the following

configuration on the client machine so the NX Check-Mate validation process can

be run from the client side.2.configure registry on the 4tier client:

e.g.:

Windows Registry Editor [HKEY_CLASSES_ROOT\.ugcheckpart]

@="ugcheckpart"

"Content Type"="application/ugcheckpart"[HKEY_CLASSES_ROOT\ugcheckpart]

[HKEY_CLASSES_ROOT\ugcheckpart\shell]

[HKEY_CLASSES_ROOT\ugcheckpart\shell\open]

[HKEY_CLASSES_ROOT\ugcheckpart\shell\open\command]

@="%tc_4-tier root directory%\check\ug_check_part.bat"3. configure ug_check_part.bat

e.g:

set UGII_UGMGR_HTTP_URL=http://fourtierhostname:80/tc

set UGII_BASE_DIR=d:\ugs\nx..

set UGII_ROOT_DIR=d:\ugs\nx..\ugii Notes

Teamcenter Documentation - Administering Teamcenter - Validation Manager Guide

Notes

KB Article ID# PL7005696

Contents

SummaryDetails

Associated Components