Remove Parameters from Drafting Sheet Curves

2021-10-06T23:27:01Z

Summary


Details

--------------- 
After using trimmed curves to manually create a table on a drawing sheet, how 
can the associativity of the curves be removed? 


Since the curves were created associatively, moving some of them also moves 
their parent curves.



Solution

There is no 'Edit --> Feature --> Remove Parameters' function available in the Drafting application.  Also, there is no 'Associative' check-box available in the edit curve parameters dialog.


A solution is to zoom in such that the table fills the monitor, then use 

File --> Export --> CGM to export the display to a file.


Delete the original curves in the table.


Import the CGM file created above.


The imported curves are no longer associative and can be moved as desired.



Notes and References





Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V1855
Function: DRAWING/VIEW

Ref: 002-7005687

KB Article ID# PL7005687

Contents

SummaryDetails

Associated Components