How to control decimal places when using Auto Weld Symbols

2021-10-06T23:26:57Z

Summary


Details

When using the command 'Insert-->Annotation-->Auto Weld Symbols', the weld 
symbols created use the incorrect number of decimal places. How can the decimal 
places in the Weld Symbols created using Auto Weld Symbols be controlled?



Solution

 This option is located in Customer Defaults. 
1. Select 'File-->Utilities-->Customer Defaults'. 
2. Expand 'Drafting'. 
3. Highlight 'Auto Weld Symbols'. 
4. On the 'General' tab, modify the setting, 'Weld Symbol Decimal Places', 
 using the slider bar. 
5. OK the Customer Defaults dialog. 
6. Exit and re-start NX for the change to take effect.


Now when a Weld Symbol is created using the 'Auto Weld Symbols' command, the 
specified number of decimal places will be used.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: KDA
Version: V8.5
Function: WELD_ASSISTANT

Ref: 002-7005677

KB Article ID# PL7005677

Contents

SummaryDetails

Associated Components