Setting the default location for the Cue/Status Line Position

2021-10-06T23:26:46Z

Summary


Details

In NX9, the default Cue/Status Line Position is placed at the bottom. 
How can the Cue/Status Line Position be placed at the top by default?



Solution

 The Cue/Status Line Position can only be changed by customizing the toolbar 
layout or in the registry.


Customizing the Toolbar Layout: 
1. Select 'Tools-->Customize'. 
2. Select the 'Layout' tab. 
3. Toggle 'Top' for the 'Cue/Status Line Position'. 
4. Close the Customize dialog. 
5. Select 'Preferences-->User Interface'. 
6. Select the 'Layout' tab. 
7. Toggle ON 'Save Layout at Exit'. 
8. OK the User Interface Preferences dialog. 
9. Exit NX to save this layout. 
10. Re-start NX. 
11. Select 'Preferences-->User Interface'. 
12. Select the 'Layout' tab. 
13. Toggle OFF 'Save Layout at Exit', so that another setting 
 does not accidentally overwrite the current layout. 
14. OK the User Interface Preferences dialog.


The Cue/Status Line Position is saved to the registry in the following 
location: 
HKEY_CURRENT_USER\Software\Unigraphics Solutions\Unigraphics 
NX\9.0\Layout\UI_Preferences\Cue 
If the value of 'Cue' is "0", the position will be set to 'Top'. 
If the value of 'Cue' is "1", the position will be set to 'Bottom'.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V9.0
Function: UI_TOOLS

Ref: 002-7005676

KB Article ID# PL7005676

Contents

SummaryDetails

Associated Components