Can I access the last 10 commands for quick easy access?
Solution
You can use Repeat Command to rerun any one of the last ten commands that you used.
When you switch to another application or a task environment in NX, the list displays the commands that you most recently used in that application or task environment in the current NX session. Each application and task environment retains its own
Repeat Command list for the duration of your NX session.
Suppose you switch between the Modeling and the Sheet Metal applications. When you are in the Modeling application, the list displays only the Modeling commands that you recently used.
Using the drop-down menu: Tools --> Repeat Command
Or Right-click in the background of the graphics window→
Repeat Command 
The last ten commands that you used appear in the Repeat Command drop-down list
in the order in which they were activated. The most recently activated command
appears at the top of the list.
You can use shortcut menu: Right-click in the background of the graphics
window --> Repeat Command. Or you can press F4 to run the last command.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V12.0
Function: UI_TOOLS
Ref: 002-7005343