Engrave/emboss text on a contour surface of a solid model

2021-10-06T23:27:13Z

Summary


Details

--------------- 
If you need to emboss or engrave text of different fonts on a solid model which has contour faces, below are the steps you can try:



Solution

 1) Creating text using the font you want using Insert --> Curve --> Text On 
Curve, (the curve could be sketch curve). Under settings, toggle on Join 
Curves.


2) Project the text onto the contour surface of the solid model using 
Insert --> Curve from Curves --> Project using Along Face Normal direction.


3) Using Divide Face function to divide the existing contour face and the 
curves from the text as dividing objects. You also want Normal to Face as 
Projection Direction. Insert --> Curve from Curves --> Project 
(If you have problem to project, you could change the tolerance to a tighter 
value).


4) Extrude individual letters using Insert --> Design Feature --> Extrude --> 
Set selection intent to Face Edges to select the Divide Face edges , then you 
can either unite or subtract to the main solid to create engraving or emboss.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0.2
Function: CURVE

Ref: 002-7005302

KB Article ID# PL7005302

Contents

SummaryDetails

Associated Components