Can one use Project Name as a note in the drawing?

2021-10-06T23:27:15Z

Summary


Details

--------------- 
In Teamcenter, one can create a Project, but can the Project Name be inserted 
into a note in a drawing?



Solution

 First, one needs to create attribute mapping with the syntax below:


PROJECT_NAME : ItemRevision.project_ids /master=iman /description="Project 
Name"


When you create new NX file, you should get the system attribute Project_Name 
in a Part Attribute. You then can insert a note using this system attribute.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V12.0.2
Function: ANNOTATION

Ref: 002-7005260

KB Article ID# PL7005260

Contents

SummaryDetails

Associated Components