For thermal boundary conditions the flow log file shows several columns of
data. The first three columns are self explanatory but I cannot find a
description for the last two. What are FSF and TCP?
Thermal Boundary Condition Type Value FSF TCP----------------------------------------------------------------------
1 - THERMAL BOUNDARY CONDIT Temperature 2.000E+02 F No No
----------------------------------------------------------------------
Solution
"FSF" refers to "flow surface" and "TCP" refers to "thermal coupling". Note
that "No" means that the selection for this thermal boundary condition is not
part of a flow surface / thermal coupling, "Yes" means that a subset of the
selection is part of a flow surface / thermal coupling, and "All" means that
all of the selection is part of a flow surface / thermal coupling.
Notes