How to match body colors in a drawing view with the solid body in Modeling application

2021-10-06T23:27:07Z

Summary


Details

Body colors in a drawing view do not match the solid body colors in the Modeling application.



Solution

  1. Hover the cursor over the drawing view border, 'MouseButton3-->Style'. 
  2. In the Style dialog, select the 'Visible Line' tab. 
  3. Select the color bar in the upper left hand corner. 
    This will display the Color dialog. 
  4. Under the Selected Color header, select the 'Deselect All Colors' icon. 
    This will reset the view colors of all the visible lines to the solid body colors. 
  5. OK the Color dialog. 
  6. OK the View Style dialog.


To set this preference in the drawing for new view, perform the following: 
  1. Select 'Preferences-->View'. 
  2. Select the 'Visible Line' tab. 
  3. Select the color bar in the upper left hand corner. 
    This will display the Color dialog. 
  4. Under the Selected Color header, select the 'Deselect All Colors' icon. 
  5. OK the Color dialog. 
  6. OK the View Preferences dialog.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V10.0
Function: DRAWING/VIEW

Ref: 002-7005028

KB Article ID# PL7005028

Contents

SummaryDetails

Associated Components