NX Unable to select a component to export to a STEP file

2021-10-06T23:26:47Z
NX for Design

Summary


Details

When exporting the entire assembly to a STEP file, the component is included in 
the exported STEP file. However, when attempting to select certain components 
for export to a STEP file, the same component is not selectable and cannot be 
included in the STEP export process.



Solution

 When selecting specific components for export to a STEP file, if the component 
is not of the same units as the assembly that is the work part, the component 
will not be selectable for export. 
The component must be of the same units as the work part assembly in order to 
be selectable for export using the STEP translator.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V7.5.5
Function: STEP_AP214

Ref: 002-7004918

KB Article ID# PL7004918

Contents

SummaryDetails

Associated Components

CAD Translators