When double clicking on a sketch to edit, NX always enters the Direct Sketch environment in NX1855.
Solution
NX8 introduced Direct Sketching. The default behavior for editing sketches is to use the Direct Sketch environment. Users can change this behavior using either of the methods below:
1. Set the preference for the current session of NX. 'Preferences --> Modeling --> Edit' and set 'Edit Sketch Action' to 'Task Environment'.

2. Set the preference for any session of NX. 'File --> Utilities --> Customer Defaults --> Modeling --> General --> Edit' and set 'Edit Sketch Action' to 'Task Environment'

Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1855
Function: SKETCHER
Ref: 002-7004793