Correcting selection problems with geometry at extreme locations

2021-10-06T23:27:09Z

Summary


Details

--------------- 
Users might experience problems selecting objects when working with an NX part file that contains geometry at extreme distances from the origin such as a large plant layout at full scale.



Solution

 The reason for this behavior is because the value for the customer default "Maximum Size for an Objects Bounding Box" is not large enough to include objects at the extremes of the part. To correct the problem make the following changes to the customer defaults:


Select File --> Utilities --> Customer Defaults 
Gateway --> Visualization --> View/Screen tab --> "Maximum Size for an Objects Bounding Box" 
 set to 39,370 in English units system 
 set to 1,000,000 in Metric units system


Save the defaults and restart NX and all objects should now be selectable.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: SYSENG
Version: V1847
Function: SELECTION

Ref: 002-7004734

KB Article ID# PL7004734

Contents

SummaryDetails

Associated Components