NX "NX has stopped working" error when opening a part in NX

2021-10-06T23:26:53Z
NX for Design

Summary


Details

--------------- 
Some cases have been reported to Siemens GTAC where users try to open an NX part and they get a message "NX has stopped working'. The NX session collapses when selecting Close or Debug from the error dialog box. There are no significant error details reported in the NX syslog file.



Solution

Siemens GTAC has determined that in some of these cases, an incorrect driver for a 3DConnexion device may have been installed. If your system has one of these devices attached you should perform the following test.


To confirm if the 3DConnexion device driver is causing the problem you must first DISABLE the device driver for the 3DConnexxion device (unplugging it is NOT sufficient) and then start NX to see if the problem persists or not. If the problem no longer occurs then it is suggested that you UNINSTALL the current driver and go to the 3DConnexion website to download and install the appropriate driver.


If you need help with disabling or installing the driver please contact 3DConnexion support for assistance.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: ASSEMBLIES
Version: V1847
Function: PART_FILE_OPS

Ref: 002-7004597

KB Article ID# PL7004597

Contents

SummaryDetails

Associated Components

Assemblies